NFC PN7150 on Qualcomm Android R integration errors, memory access error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC PN7150 on Qualcomm Android R integration errors, memory access error

661件の閲覧回数
smile123
Contributor I

We face following issue with respect to NFC.

 
We are using PN7150 NFC on Qualcomm based chipset running android R with sn100 hal. While enabling the pn7150 using sn100 android stack we are facing issues. Once we enable the NFC we could see RF side active with 13.5 MHz clock. But we are not able to detect NFC card / tag.
From log we can see some command responses to the i2c chip with the syntax errors in the responses.. we are not certain whether this error response from device is causing detection failures or is it because of configuration not right done initially from the software.
 
 
We would like to know why the error is coming and how to prevent it. error prints are below.?
 
Does sn100 libraries on android R support PN7150.? Are there any customizations needed?
 
 
09-29 11:15:22.397   666   666 D vendor.nxp.hardware.nfc@2.0-service: nxp_rf_config_path=/system/vendor/libnfc-nxp_RF.conf
09-29 11:15:22.398   666   666 D vendor.nxp.hardware.nfc@2.0-service: Fw_Lib_Path=/system/vendor/lib/libsn100u_fw.so
09-29 11:15:22.400   666   666 D NxpHal  : Error : opening (/system/vendor/lib64/libonebinary.so) !!
09-29 11:15:22.400   666   666 D NxpHal  : nfc_debug_enabled : 1
09-29 11:15:22.400   666   666 D NxpExtns: find found NXPLOG_NCIHAL_LOGLEVEL=(0x3)
09-29 11:15:22.401   666   666 D NxpExtns: find found NXPLOG_EXTNS_LOGLEVEL=(0x3)
09-29 11:15:22.401   666   666 D NxpExtns: find found NXPLOG_TML_LOGLEVEL=(0x3)
09-29 11:15:22.401   666   666 D NxpExtns: find found NXPLOG_FWDNLD_LOGLEVEL=(0x3)
09-29 11:15:22.401   666   666 D NxpExtns: find found NXPLOG_NCIX_LOGLEVEL=(0x3)
09-29 11:15:22.401   666   666 D NxpExtns: find found NXPLOG_NCIR_LOGLEVEL=(0x3)
09-29 11:15:22.401   666   666 D NxpNfcHal: phNxpLog_InitializeLogLevel: global =1, Fwdnld =3, extns =3,                 hal =3, tml =3, ncir =3,                 ncix =3
09-29 11:15:22.401   666   666 D NxpExtns: find found MIFARE_READER_ENABLE=(0x1)
09-29 11:15:22.403   666   666 D NxpHal  : Entering phNxpNciHal_init_monitor
09-29 11:15:22.403   666   666 D NxpHal  : Returning with SUCCESS
09-29 11:15:22.403   666   666 D NxpExtns: find found NXP_NFC_DEV_NODE=/dev/pn544
09-29 11:15:22.403   666   666 D NxpTml  : Opening port=/dev/pn544
09-29 11:15:22.404   666   666 D NxpTml  : phTmlNfc_i2c_reset(), VEN level 7
09-29 11:15:22.412     0     0 I pn54x_dev_open: 10,62
09-29 11:15:22.431  3946  3969 I omm.location.X: Background young concurrent copying GC freed 5682(494KB) AllocSpace objects, 2(40KB) LOS objects, 93% free, 1757KB/25MB, paused 162us total 115.626ms
09-29 11:15:22.435  4035  4035 I d.process.acor: The ClassLoaderContext is a special shared library.
09-29 11:15:22.457   941  1220 I chatty  : uid=1000(system) android.bg expire 3 lines
09-29 11:15:22.457     0     0 I         : pn54x_dev_ioctl, cmd=1074063617, arg=7
09-29 11:15:22.457     0     0 E         : pn54x_dev_ioctl bad SET_PWR arg 7 error override
09-29 11:15:22.473     0     0 I         : pn54x_dev_ioctl, cmd=59652, arg=5138418468164818527
09-29 11:15:22.473     0     0 E         : pn54x_dev_ioctl bad ioctl 59652 error override
09-29 11:15:22.474   666   666 D NxpTml  : phTmlNfc_get_platform: interface = 0
09-29 11:15:22.477   666  4159 D NxpTml  : PN54X - Tml Reader Thread Started................
09-29 11:15:22.479   666  4162 D NxpHal  : thread started
09-29 11:15:22.480   666  4159 D NxpTml  : PN54X - Read requested.....
09-29 11:15:22.480   666  4159 D NxpTml  : PN54X - Invoking I2C Read.....
09-29 11:15:22.494   666  4160 D NxpTml  : PN54X - Tml Writer Thread Started................
09-29 11:15:22.494   666  4160 D NxpTml  : PN54X - Tml Writer Thread Running................
09-29 11:15:22.494   666  4160 D NxpTml  : PN54X - Write requested.....
09-29 11:15:22.494   666  4160 D NxpTml  : PN54X - Invoking I2C Write.....
09-29 11:15:22.496   666  4160 D NxpNciX : len =   4 > 20000100
09-29 11:15:22.497   666  4160 D NxpTml  : PN54X - I2C Write successful.....
09-29 11:15:22.497   666  4160 D NxpTml  : PN54X - Posting Fresh Write message.....
09-29 11:15:22.497   666  4160 D NxpTml  : PN54X - Tml Writer Thread Running................
09-29 11:15:22.497   666  4162 D NxpHal  : write successful status = 0x0
09-29 11:15:22.497   666   666 D NxpHal  : Response timer started
09-29 11:15:22.497   666   666 D NxpHal  : Waiting after ext cmd sent
09-29 11:15:22.501   666  4159 D NxpTml  : PN54X - I2C Read successful.....
09-29 11:15:22.501   666  4159 D NxpNciR : len =   6 > 400003001100
09-29 11:15:22.501   666  4159 D NxpTml  : PN54X - Posting read message.....
09-29 11:15:22.501   666  4162 D NxpHal  : read successful status = 0x0
09-29 11:15:22.502   666  4162 D NxpHal  : CORE_RESET_RSP NCI1.0
09-29 11:15:22.502   666   666 D NxpHal  : Response timer stopped
09-29 11:15:22.502   666   666 D NxpHal  : Checking response
09-29 11:15:22.502   666  4159 D NxpTml  : PN54X - Read requested.....
09-29 11:15:22.503   666  4159 D NxpTml  : PN54X - Invoking I2C Read.....
09-29 11:15:22.503   666  4160 D NxpTml  : PN54X - Write requested.....
09-29 11:15:22.503   666  4160 D NxpTml  : PN54X - Invoking I2C Write.....
09-29 11:15:22.506   666  4160 D NxpNciX : len =   3 > 200100
09-29 11:15:22.506   666  4160 D NxpTml  : PN54X - I2C Write successful.....
09-29 11:15:22.506   666  4160 D NxpTml  : PN54X - Posting Fresh Write message.....
09-29 11:15:22.507   666  4160 D NxpTml  : PN54X - Tml Writer Thread Running................
09-29 11:15:22.507   666  4162 D NxpHal  : write successful status = 0x0
09-29 11:15:22.508   666   666 D NxpHal  : Response timer started
09-29 11:15:22.509   666   666 D NxpHal  : Waiting after ext cmd sent
09-29 11:15:22.509   666  4159 D NxpTml  : PN54X - I2C Read successful.....
09-29 11:15:22.509   666  4159 D NxpNciR : len =  28 > 40011900031E030008000102038081828302D002FF020004881001AE
09-29 11:15:22.509   666  4159 D NxpTml  : PN54X - Posting read message.....
09-29 11:15:22.510   666  4162 D NxpHal  : read successful status = 0x0
09-29 11:15:22.510   666  4162 D NxpHal  : CORE_INIT_RSP NCI1.0 received !
09-29 11:15:22.510   666  4162 D NxpHal  : processChipType HwVersion : 0x88
09-29 11:15:22.510   666  4162 D NxpHal  : processChipType Product : PN548C2
09-29 11:15:22.510   666  4162 D NxpHal  : phNxpNciHal_configFeatureList ()chipType = 3
09-29 11:15:22.511   666  4162 D NxpHal  : phNxpNciHal_configFeatureList ()chipType = 3
09-29 11:15:22.511   666  4162 D NxpHal  : phNxpNciHal_configFeatureList ()FW = 1
09-29 11:15:22.511   666  4162 D NxpHal  : NxpNci> FW Version: 10.1.ae
09-29 11:15:22.511   666   666 D NxpHal  : Response timer stopped
09-29 11:15:22.511   666   666 D NxpHal  : Checking response
09-29 11:15:22.512   666   666 D NxpExtns: find found NXP_I2C_FRAGMENTATION_ENABLED=(0x0)
09-29 11:15:22.512   666   666 D NxpFwDnld: I2C status : 0
09-29 11:15:22.512   666  4160 D NxpTml  : PN54X - Write requested.....
09-29 11:15:22.512   666  4159 D NxpTml  : PN54X - Read requested.....
09-29 11:15:22.512   666  4159 D NxpTml  : PN54X - Invoking I2C Read.....
09-29 11:15:22.512   666  4160 D NxpTml  : PN54X - Invoking I2C Write.....
09-29 11:15:22.514   666  4160 D NxpNciX : len =   6 > 20030301A005
09-29 11:15:22.514   666  4160 D NxpTml  : PN54X - I2C Write successful.....
09-29 11:15:22.514   666  4160 D NxpTml  : PN54X - Posting Fresh Write message.....
09-29 11:15:22.515   666  4160 D NxpTml  : PN54X - Tml Writer Thread Running................
09-29 11:15:22.515   666  4162 D NxpHal  : write successful status = 0x0
09-29 11:15:22.515   666   666 D NxpHal  : Response timer started
09-29 11:15:22.515   666   666 D NxpHal  : Waiting after ext cmd sent
09-29 11:15:22.516   666  4159 D NxpTml  : PN54X - I2C Read successful.....
09-29 11:15:22.517   666  4159 D NxpNciR : len =   9 > 4003060001A0050100
09-29 11:15:22.517   666  4159 D NxpTml  : PN54X - Posting read message.....
09-29 11:15:22.517   666  4162 D NxpHal  : read successful status = 0x0
09-29 11:15:22.517   666  4162 D NxpHal  : phNxpNciHal_print_res_status: response status =STATUS_OK
09-29 11:15:22.519   666   666 D NxpHal  : Response timer stopped
09-29 11:15:22.519   666   666 D NxpHal  : Checking response
09-29 11:15:22.519   666   666 D NxpHal  : phNxpNciHal_CheckFwRegFlashRequired() : enter
09-29 11:15:22.519   666   666 D NxpFwDnld: Allocating Mem for Dnld Context..
09-29 11:15:22.519   666   666 E NxpFwDnld: phDnldNfc_SetDlRspTimeout timeout value =9c4
09-29 11:15:22.520   666   666 D NxpExtns: find found NXP_FW_TYPE=(0x1)
09-29 11:15:22.520   666   666 D NxpFwDnld: firmware type from conf file: 1
09-29 11:15:22.521   666  4159 D NxpTml  : PN54X - Read requested.....
09-29 11:15:22.521   666  4159 D NxpTml  : PN54X - Invoking I2C Read.....
09-29 11:15:22.532  4084  4084 I Perf    : Connecting to perf service.
09-29 11:15:22.559  4084  4084 D NetworkSecurityConfig: No Network Security Config specified, using platform default
09-29 11:15:22.561  4084  4084 D NetworkSecurityConfig: No Network Security Config specified, using platform default
09-29 11:15:22.565   425   425 I hwservicemanager: getTransport: Cannot find entry vendor.qti.hardware.iop@2.0::IIop/default in either framework or device manifest.
09-29 11:15:22.566  1098  1098 E ANDR-IOP: IIop:: Iop HAL Service is not available.
09-29 11:15:22.580  4128  4128 I .localtranspor: The ClassLoaderContext is a special shared library.
09-29 11:15:22.582  4084  4084 I WigigBootCompleteReceiver: onReceive: got Intent { act=android.intent.action.BOOT_COMPLETED flg=0x89000010 cmp=com.qualcomm.qti.server.wigigapp/.BootCompleteBroadcastReceiver (has extras) }
09-29 11:15:22.601  4084  4084 I WigigSettingsService: onCreate
09-29 11:15:22.601   666   666 D NxpFwDnld: @@@/system/vendor/lib/libsn100u_fw.so
09-29 11:15:22.602   666   666 D NxpFwDnld: FW Image Length - ImageInfoLen 204518
09-29 11:15:22.602   666   666 D NxpFwDnld: FW Image Info Pointer - pImageInfo 0x74b2733488
09-29 11:15:22.602   666   666 D NxpFwDnld: FW Major Version Num - 10
09-29 11:15:22.602   666   666 D NxpFwDnld: FW Minor Version Num - 57
09-29 11:15:22.602   666   666 D NxpFwDnld: FW Image Length - 204518
09-29 11:15:22.603   666   666 D NxpFwDnld: FW Image Info Pointer - 0x74b2733488
09-29 11:15:22.603   666   666 D NxpHal  : FW version of the libsn100u.so binary = 0x1057
09-29 11:15:22.603   666   666 D NxpHal  : FW version found on the device = 0x1001ae
09-29 11:15:22.604  2124  2124 D KeyguardViewMediator: adjustStatusBarLocked: mShowing=true mOccluded=false isSecure=false force=false --> flags=0x1200000
09-29 11:15:22.604   666   666 D NxpHal  : Flash option not found; giving default value
09-29 11:15:22.606  2124  2124 D StatusBar: disable<e i a s b H R c s > disable2<q i n >
09-29 11:15:22.609  4084  4084 E WigigManager: Wigig service not available
09-29 11:15:22.610  4084  4084 E WigigSettingsService: Failed to get WigigManager instance
09-29 11:15:22.611   941   941 I chatty  : uid=1000(system) Binder:941_3 expire 4 lines
09-29 11:15:22.616   666   666 D NxpHal  : FW update not required
09-29 11:15:22.616   666   666 D NxpFwDnld: Freeing Mem for Dnld Context..
09-29 11:15:22.617  2357  2357 D ApplicationLoaders: Returning zygote-cached class loader: /system/framework/android.test.base.jar
09-29 11:15:22.617   666   666 D NxpHal  : phNxpNciHal_CheckFwRegFlashRequired() : exit - status = 0 wFwUpdateReq=0, wRfUpdateReq=0
09-29 11:15:22.617   666   666 D NxpHal  : FW update not required
09-29 11:15:22.618   666   666 D NxpHal  : property_set_intf, key[nfc.fw.downloadmode_force], value[0]
09-29 11:15:22.618   666   666 D NxpHal  : phNxpNciHal_setSystemProperty : Enter Key = nfc.fw.downloadmode_force, value = 0
09-29 11:15:22.618   666   666 E NxpHal  : phNxpNciHal_conf_nfc_forum_mode: command is not provided
09-29 11:15:22.619   666  4160 D NxpTml  : PN54X - Write requested.....
09-29 11:15:22.619   666  4160 D NxpTml  : PN54X - Invoking I2C Write.....
09-29 11:15:22.621   666  4160 D NxpNciX : len =   6 > 20030301A068
09-29 11:15:22.621   666  4160 D NxpTml  : PN54X - I2C Write successful.....
09-29 11:15:22.622   666  4160 D NxpTml  : PN54X - Posting Fresh Write message.....
09-29 11:15:22.622   666  4160 D NxpTml  : PN54X - Tml Writer Thread Running................
09-29 11:15:22.622   666  4162 D NxpHal  : write successful status = 0x0
09-29 11:15:22.623   666  4159 D NxpTml  : PN54X - I2C Read successful.....
09-29 11:15:22.626   666  4159 D NxpNciR : len =   9 > 4003060001A0680100
09-29 11:15:22.626   666  4159 D NxpTml  : PN54X - Posting read message.....
09-29 11:15:22.627   666  4162 D NxpHal  : read successful status = 0x0
09-29 11:15:22.627   666  4162 D NxpHal  : phNxpNciHal_print_res_status: response status =STATUS_OK
09-29 11:15:22.628   666  4159 D NxpTml  : PN54X - Read requested.....
09-29 11:15:22.628   666  4159 D NxpTml  : PN54X - Invoking I2C Read.....
09-29 11:15:22.634   666   666 D NxpHal  : Response timer started
09-29 11:15:22.634   666   666 D NxpHal  : Waiting after ext cmd sent
09-29 11:15:22.634   666   666 D NxpHal  : Response timer stopped
09-29 11:15:22.634   666   666 D NxpHal  : Checking response
09-29 11:15:22.635   666  4160 D NxpTml  : PN54X - Write requested.....
09-29 11:15:22.635   666  4160 D NxpTml  : PN54X - Invoking I2C Write.....
09-29 11:15:22.638   666  4160 D NxpNciX : len =  49 > 20022E01A0680100000102038081828382D002FF020004881001AE00000000000000000000000000000000000000000000
09-29 11:15:22.638   666  4160 D NxpTml  : PN54X - I2C Write successful.....
09-29 11:15:22.638   666  4160 D NxpTml  : PN54X - Posting Fresh Write message.....
09-29 11:15:22.639   666  4160 D NxpTml  : PN54X - Tml Writer Thread Running................
09-29 11:15:22.639   666  4162 D NxpHal  : write successful status = 0x0
09-29 11:15:22.639   666   666 D NxpHal  : Response timer started
09-29 11:15:22.639   666   666 D NxpHal  : Waiting after ext cmd sent
09-29 11:15:22.642   666  4159 D NxpTml  : PN54X - I2C Read successful.....
09-29 11:15:22.642   666  4159 D NxpNciR : len =   5 > 4002020500
09-29 11:15:22.642   666  4159 D NxpTml  : PN54X - Posting read message.....
09-29 11:15:22.642   666  4162 D NxpHal  : read successful status = 0x0
09-29 11:15:22.643   666  4162 D NxpHal  : phNxpNciHal_print_res_status: response status =STATUS_SYNTAX_ERROR
09-29 11:15:22.643   666   666 D NxpHal  : Response timer stopped
09-29 11:15:22.643   666   666 D NxpHal  : Checking response
09-29 11:15:22.643   666   666 D NxpHal  : phNxpNciHal_MinOpen(): exit
09-29 11:15:22.644   666   666 D android.hardware.nfc@1.2-impl: Nfc::open Exit
09-29 11:15:22.644  4035  4035 I ContactsPerf: VoicemailContentProvider.onCreate start
09-29 11:15:22.645   666  4159 D NxpTml  : PN54X - Read requested.....
09-29 11:15:22.645   666  4159 D NxpTml  : PN54X - Invoking I2C Read.....
09-29 11:15:22.648  3726  3829 I libnfc_nci: [INFO:NfcAdaptation.cc(1035)] NfcAdaptation::HalDownloadFirmwareCallback: event=0x0
09-29 11:15:22.649  3726  3829 I libnfc_nci: [INFO:NfcAdaptation.cc(1051)] NfcAdaptation::HalDownloadFirmwareCallback: HAL_NFC_OPEN_CPLT_EVT
09-29 11:15:22.651  3726  4140 I libnfc_nci: [INFO:NfcAdaptation.cc(855)] HalWriteIntf: Enter
09-29 11:15:22.652  3726  4140 I libnfc_nci: [INFO:NfcAdaptation.cc(704)] NfcAdaptation::HalWrite
09-29 11:15:22.658   666  4160 D NxpTml  : PN54X - Write requested.....
09-29 11:15:22.658   666  4160 D NxpTml  : PN54X - Invoking I2C Write.....
09-29 11:15:22.660   666  4160 D NxpNciX : len =   4 > 20000100
09-29 11:15:22.660   666  4160 D NxpTml  : PN54X - I2C Write successful.....
09-29 11:15:22.660   666  4160 D NxpTml  : PN54X - Posting Fresh Write message.....
09-29 11:15:22.661   666  4160 D NxpTml  : PN54X - Tml Writer Thread Running................
09-29 11:15:22.661   666  4162 D NxpHal  : write successful status = 0x0
09-29 11:15:22.664   666  4159 D NxpTml  : PN54X - I2C Read successful.....
09-29 11:15:22.665   666  4159 D NxpNciR : len =   6 > 400003001100
09-29 11:15:22.665   666  4159 D NxpTml  : PN54X - Posting read message.....
09-29 11:15:22.665   666  4162 D NxpHal  : read successful status = 0x0
09-29 11:15:22.665   666  4162 D NxpHal  : CORE_RESET_RSP NCI1.0
09-29 11:15:22.665  4128  4128 I Perf    : Connecting to perf service.
09-29 11:15:22.666  3726  3829 I libnfc_nci: [INFO:NfcAdaptation.cc(1115)] HalDownloadFirmwareDataCallback: enter
09-29 11:15:22.666  3726  3829 I libnfc_nci: [INFO:nfc_ncif.cc(1554)] CORE_RESET_RSP len :0x3
09-29 11:15:22.666  3726  3829 I libnfc_nci: [INFO:nfc_ncif.cc(398)] nfc_ncif_send_cmd()
09-29 11:15:22.666  3726  3829 I libnfc_nci: [INFO:nfc_ncif.cc(315)] nfc_ncif_check_cmd_queue : making p_buf NULL.
09-29 11:15:22.667   666  4159 D NxpTml  : PN54X - Read requested.....
09-29 11:15:22.667   666  4159 D NxpTml  : PN54X - Invoking I2C Read.....
09-29 11:15:22.693   941  4166 I chatty  : uid=1000(system) Binder:941_3 expire 1 line
09-29 11:15:22.698  4128  4128 D NetworkSecurityConfig: No Network Security Config specified, using platform default
09-29 11:15:22.699  4128  4128 D NetworkSecurityConfig: No Network Security Config specified, using platform default
09-29 11:15:22.703   425   425 I hwservicemanager: getTransport: Cannot find entry vendor.qti.hardware.iop@2.0::IIop/default in either framework or device manifest.
09-29 11:15:22.704  1098  1098 E ANDR-IOP: IIop:: Iop HAL Service is not available.
09-29 11:15:22.706   941  4166 I DropBoxManagerService: add tag=SYSTEM_BOOT isTagEnabled=true flags=0x2
09-29 11:15:22.717  4035  4035 I ContactsPerf: VoicemailContentProvider.onCreate finish
09-29 11:15:22.717   941  4166 I BootReceiver: Copying audit failures to DropBox
09-29 11:15:22.727   941  4166 I BootReceiver: Checking for fsck errors

 
0 件の賞賛
0 返答(返信)