NFC Ntag216 bump connect question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Ntag216 bump connect question

1,195 Views
r_chen
Contributor I

HI sir,

We are working NFC chip of Ntag216 & 213 to make flip-chip process into etching antenna inlay, a question about the chip connect position, if bump LA to connect with GND and LB to connect TP (as like photo) is it can work function? have any risk? 

01.jpg

0 Kudos
Reply
2 Replies

1,099 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Rod,

The LA and LB are Antenna connection LA and  Antenna connection LB.
Should not connect other pads with them.
Please refer the NTAG IC connections of NTAG Antenna Design Guide.

NTAG IC connections.png

 

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,099 Views
r_chen
Contributor I

HI Robin, 

thanks for your information...

0 Kudos
Reply