Hello,
We have a problem when we try to send a mutual authentication with Inlays ICODE DNA.
We did the key initialization as mentioned in the doc : -
What is the problem in the process ? Is there a missing step ?
Could you help us ?
Thanks
Regards,
S.L
I am at the same situation right now. After valid MAM1 response from the tag, I have used the website provided in the AN11808 document to compute the MAM2 message and sent to the tag. I can see the data sent on the scope which is correct. But there is no response from the tag. Anything to do with the delay in sending the MAM2 message after valid MAM1 response from tag?
Hello Gireesh,
Your numericals are ok. Authenticate command takes approx. 8,5ms, AES calculation on the Tag takes 4ms, length of the Tag´s response shall be 7ms, then you can expect a valid answer.
Do you have any chance to capture the RF on oscilloscope?
Best regards,
Uros
I am only interested to know if there is any timeout applied to the authentication commands like, after MAM1 is sent out and responded by the tag, if MAM2 is not received within xx seconds, or if MAM2 is received after xx seconds, the authentication is aborted. Otherwise, I am just polling for the tag response and I allowing plenty of time for tag to respond.
We don't have facility to capture RF signal, I am working on that to see if we can get one shortly.
Dear Sebastien,
Yes like you stated, you have to do a decrypt before.
DECRYPT (the tag can only do ENCRYPT): 59 F3 B5 DC C2 1F 77 FA 31 8E 67 E7 19 67 DD 99
Please note (important):
ISO15693 as air interface, is defined as LSB first, but crypto suite is defined as MSB first in our case.
Hopefully it works now for you.
br,
Uros
I tried decryption as well, but still got unknown error response...
Here is what I am doing
Key: 1A 31 06 F0 D9 BA 90 E3 4F 29 E3 3B C0 FF 77 DB
Challenge: 00 00 00 00 00 00 00 00 00 00
Response from tag:
A7 55 07 B3 45 F4 89 5D 08 19 F8 CB DF 5B BD E5 1C 2D 5F 7A A5 FB 98
Swapped response: (excluding baker filed)
98 FB A5 7A 5F 2D 1C E5 BD 5B DF CB F8 19 08 5D       89 F4 45 B3 07 55
Decrypted firts 16 bytes of swapped response
DA 83  F0 74 FF 87   00 00 00 00 00 00 00 00 00 00
MAM2
DA 80  00 00 00 00  89 F4 45 B3 07 55     F0 74 FF 87
Decrypted MAM2 
70 50 FC D4 6C 6A F3 09 56 11 65 3B 91 96 21 6A
Swapped response
00 06 6A 21 96 91 3B 65 11 56 09 F3 6A 6C D4 FC 50 70
Response from tag:
0F
Is there are any prerequisite to mutual authentication that Ia m missing here ?
I have
Config header = 81
Global crypto header = C1
Crypto configuration header = 81
Key header = C3
Key privileges = 00
is there any timing restriction like the tag is expecting response with in certain time window ?
Dear Sebastien,
Please kindly excuse for the delay. I accidentially replied to wrong topic. Hopefully you solved the issue.
I would suggest you to use some of our available SW tools. I would highly suggest NxpReaderLib available on DocStore under MIFARE SW directory, to be used with CM1 reader or Pegoda 701 (if you have it). It has a very nice Mutual Authentication example. It does all calculation for you.
Also we offer in NFC reader library - which is applicable for our reader development boards - an example to perform mutual authentication on ISO15693 protocol.
Recommendations:
Best regards,
Uros
I think I found the problem
When you send the MAM1 message , you have to decrypt the message before to send MAM2. That's ok
But before sending the MAM2 message , instead of encrypt the message , you have to decrypt it again ... logical :smileysad:
I am also at same point as you, I tried many things but no success. Trying to contact NXP support in all possible ways, but never heard back from anybody.
Hello,
Thanks for your reply.
After posting the first message , I refer to the example in AN11808 and it’s better for MAM1
In fact , it was the order bit of the MAM1 message , more precisely an inversion between AuthMethod , Step, and MAM1_RFU
Now I have a valid response for MAM1 Response , so I tried to send the second parts of mutual authentication , and I have an error , always the same message 0x01 0x0F L
I will explain more :
My key : FFEEDDCCBBAA99887766554433221100
My IChallenge_MAM1 : 00000000000000000000
I receive the following MAM1 response from the tag : 04 47 0F C3 9A 72 43 8D EC 40 08 18 95 65 27 DA F2 75 F8 08 48 6B 0A 59
What did I do wrong ?
Thanks
may be check the Key0 byte order, it expects MSByte first. Other fields to look for is
Authentication method, step number and Key ID, again byte order of all these fields. Refer to the example in AN11808.