More than one TDA8029 in I2C bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

More than one TDA8029 in I2C bus

1,163件の閲覧回数
mariocruz
Contributor I

Hi!

 

 I want to desing a dual contact smart card reader managed by I2c bus. I ´d like to use two TDA8029 ic, but it only has one fixed i2c address. How can I set a different I2c address to one of them for using more than one in parallel?

Thanks a lot!

0 件の賞賛
返信
1 返信

992件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

It only has one fixed I2C address (0x50). Fortunately, it can also be interfaced through RS232. The host interface is chosen by connecting P17 to VDD for RS232 or to GND for I2C.

Please refer to chapter 2.2 Host Controller Interface of the following document:

https://www.nxp.com/docs/en/application-note/AN10207.pdf

 

I hope this helps.

 

Regards,

Ivan.

0 件の賞賛
返信