Hi all,
We're trying out the OM27462CDK (PN7462 Controller Development Kit) to get get some experience before we are going to design our own custom board based on the PN7462 for our project.
The download of SW368322_v05.21.00 was successfull and the example "PN7462AU_ex_phExMain" runs fine with McuXpresso as within Keil ARM-MDK.
Trying to take it a step further, using Config Tools to discover how pin, clock and peripheral configuration would work out resulted in an error.
The .metadata\.log indicates:
!ENTRY com.crt.log 4 -1 2019-06-05 10:40:33.214
!MESSAGE The project 'PN7462AU_ex_phExMain' has no nature com.nxp.mcuxpresso.core.datamodels.sdkNature
!STACK 0
java.lang.Exception: org.eclipse.core.runtime.CoreException: The project 'PN7462AU_ex_phExMain' has no nature com.nxp.mcuxpresso.core.datamodels.sdkNature
at com.crt.utils.general.Reporter.log(Reporter.java:654)
at com.nxp.mcuxpresso.core.datamodels.providers.AddonsAdapterFactory.getAdapter(AddonsAdapterFactory.java:29)
at org.eclipse.core.internal.adapter.AdapterFactoryProxy.getAdapter(AdapterFactoryProxy.java:82)
at org.eclipse.core.internal.runtime.AdapterManager.getAdapter(AdapterManager.java:295)
at com.nxp.swtools.mcuxpressoide.adapter.MCUXpressoIDEAdapter.<init>(MCUXpressoIDEAdapter.java:53)
at com.nxp.swtools.mcuxpressoide.adapter.MCUXpressoIDEAdapterFactory.getAdapter(MCUXpressoIDEAdapterFactory.java:32)
at org.eclipse.core.internal.adapter.AdapterFactoryProxy.getAdapter(AdapterFactoryProxy.java:82)
at org.eclipse.core.internal.runtime.AdapterManager.getAdapter(AdapterManager.java:295)
at com.nxp.swtools.sdkproject.ToolchainProjectFactory.createToolchainProjectForImport(ToolchainProjectFactory.java:51)
at com.nxp.swtools.eclipse.handlers.OpenMexForProject.lambda$1(OpenMexForProject.java:123)
at org.eclipse.jface.operation.ModalContext$ModalContextThread.run(ModalContext.java:119)
Caused by: org.eclipse.core.runtime.CoreException: The project 'PN7462AU_ex_phExMain' has no nature com.nxp.mcuxpresso.core.datamodels.sdkNature
at com.nxp.mcuxpresso.core.datamodels.providers.SDKComponentsHandler.internalRefresh(SDKComponentsHandler.java:105)
at com.nxp.mcuxpresso.core.datamodels.providers.SDKComponentsHandler.<init>(SDKComponentsHandler.java:100)
at com.nxp.mcuxpresso.core.datamodels.providers.AddonsAdapterFactory.getAdapter(AddonsAdapterFactory.java:27)
... 9 more
!ENTRY com.nxp.swtools.eclipse.handlers 4 0 2019-06-05 10:40:33.288
!MESSAGE Eclipse Project not accessible. See Project Explorer, Problems View or Error Log for details
Can you please indicate if Config Tools within McuXpresso is supported for the PN7462?
Is there an indication when PN7462 will be supported by SDK Builder?
KInd regards,
Robert
Actually it is more like a MCUXpresso topic, and the answer is no . If you refer to MCUXpresso Config Tools|Software Development for NXP Microcontrollers (MCUs) | NXP , you may find the following info:
Since OM27462CDK is not supported by the SDK Builder, so you can not use this tool based on that board.
Hope that makes sense,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------