May I set CLRC663 RF alaways on?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

May I set CLRC663 RF alaways on?

843 Views
gogopass
Contributor I

Hello Sir:

I have a card reader project with CLRC663.

Because of special card it need more power,

I need to set the RF field always on else RF field  reset.

Does CLRC663 have any note to attention?

Or it's dangerous in this condition?

Thank your any reply .

Labels (2)
1 Reply

687 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Carlos,

It is ok to switch on RF filed out of reset, just make sure the max ITVDD within the spec. For CLRC66301 and CLRC66302 , it is 250mA and for CLRC66303 it is 500mA.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------