Linux experts: neard nfc daemon has error. Any clues as to why?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux experts: neard nfc daemon has error. Any clues as to why?

1,146件の閲覧回数
danielwinsor
Contributor II

been try to solve this for a week.   If anyone has any clue as to why neard doesn't work it would

be appreciated.

bluetooth /dev/hci0 works with bluetoothctl.

nfcDemoApp works and there is a /dev/pn544

neard[957]: ../neard-0.16/src/bluetooth.c:bt_connect() connection 0xe3560 with 0x4ab84
neard[957]: ../neard-0.16/src/bluetooth.c:register_bluez()
neard[957]: ../neard-0.16/src/bluetooth.c:bt_refresh_adapter_props() 0xe3560 0x4ab84
neard[957]: ../neard-0.16/src/bluetooth.c:bt_generic_call() DefaultAdapter
neard[957]: ../neard-0.16/src/bluetooth.c:bt_get_default_adapter_cb()
neard[957]: Could not get Bluetooth default adapter Method "DefaultAdapter" with signature "" on interface "org.bluez.Manager" doesn't exist

my source for bluetooth.c has the defaults

here is a partial output from dbus-monitor --system   when I run bluetoothctl.

   string "type='signal',sender='org.bluez',path_namespace='/org/bluez'"
[bluetooth]# method return time=1549209068.970159 sender=org.freedesktop.DBus -> destination=:1.10 serial=7 reply_serial=6
method call time=1549209068.970721 sender=:1.10 -> destination=org.bluez serial=7 path=/; interface=org.freedesktop.DBus.ObjectManager; member=GetManagedObjects
method return time=1549209068.976106 sender=:1.0 -> destination=:1.10 serial=40 reply_serial=7
   array [
      dict entry(
         object path "/org/bluez"
         array [
            dict entry(
               string "org.freedesktop.DBus.Introspectable"
               array [
               ]
            )
            dict entry(
               string "org.bluez.AgentManager1"
               array [
               ]
            )
            dict entry(
               string "org.bluez.ProfileManager1"
               array [
               ]
            )
         ]
      )
      dict entry(
         object path "/org/bluez/hci0"
         array [
            dict entry(
               string "org.freedesktop.DBus.Introspectable"
               array [
               ]
            )
            dict entry(
               string "org.bluez.Adapter1"
               array [
                  dict entry(
                     string "Address"
                     variant                         string "3C:A3:08:C3:12:9B"
                  )
                  dict entry(
                     string "AddressType"
      

0 件の賞賛
返信
0 返答(返信)