Library for CLRC663 and Kinetis (KDS).

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Library for CLRC663 and Kinetis (KDS).

839 次查看
cerma
Contributor IV

Hello everybody,

I am using FrontEnd CLRC663 and Kinetis MK61. I would like to start using library NFCReaderLibraryForCLEV663B-04.030.00.011627. BAL layer is written for processors LPC. Are you going to write it for Kinetis and project for KDS as well? If so when it will be released? If not, is there any list of components and their settings in BAL layer? For example: 4 timers are used. First is set to ...microseconds, etc. It would be easier than pull this things out of code for LPC.

Thank you.

Jaroslav

标记 (5)
0 项奖励
1 回复

495 次查看
isaacavila
NXP Employee
NXP Employee

Hello,

NFC library was planned to be migrated to Kinetis family by the end of december (https://community.nxp.com/thread/431919 ).

I will let you know as soon as this release is available.

Regards,

Isaac

0 项奖励