Hello, I've got a university project with NFC and I'm asking myself if it is possible to program it with KEIL and ULINK2.
If not is someone have a clue in order to program it? I've planned to use the µC with a raspberry Pi 3.
Yes, it is possible. Please download the PSP package for this part from https://nxp.flexnetoperations.com/control/frse/download?element=10404867 and after installation you may find the keil device pack file in the following folder:
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------