Information regarding SL3S1013FTB0 PIN information

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Information regarding SL3S1013FTB0 PIN information

918 次查看
anadeem_msee19rimms
Contributor I

I want to use SL3S1013FTB0 (G2iM+) series IC but I need information regarding RFP, RFN and OUT pin. I want to use the IC with external supply mode where I will connect DC supply positive terminal with VDD but where I will connect my ground? Another query is where I will connect antenna terminals with the IC. What is RFP and RFN and how can I connect my tag antenna RF pins to the IC pins and where. Please guide me so I can use the IC with correct pin configuration. 

0 项奖励
回复
1 回复

908 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

For the connection of the pins please refer to 2.3 Schematic diagram of the application note as the link.
URL:https://www.nxp.com/docs/en/application-note/AN11237.pdf.
Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复