Hi,
Questions about PN7150.
if we do not use NCI interface, could nxp can provide firmware to us, we can develop it further. As follows:
1. Kernel chip data;
2. RF control interface and register data;
3. Core and RF connection.
Hi Troy Liu,
unfortunately it's not possible to provide the firmware of PN7150.
However, if you need to have detailed control of the RF related register setting, I recommend either the open controller PN7362 [1] or the PN5180 NFC frontend. Both devices offer a high degree of freedom to modify the RF settings.
Hope that helps,
Michael Neurohr
[1] PN7462 Family | NFC Cortex-M0 low-power microcontroller for access control|NXP