How to write session registers in NT3H1101

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to write session registers in NT3H1101

901 次查看
burakkabasakal
Contributor I

Hello, 

Here I want to work with Pass-through mode. Here I need to modify the PTHRU_ON_OFF bit. But I have a problem to write this bit. 

I am able to read session registers. It's sequence is readed from datasheet. It's

start '0' -

write(FEh) -

write(00h (for NC_reg)-

stop

start '1'

read

stop

However , when I trying to writing in same place, I have a problem. I am doing also same sequence in datasheet, its

start '0' -

write(FEh)

write(00h (for NC_reg)-

write(02h)(for FD_ON also tried others byte)

write(01h)(to enable this bit)

stop

Can you help me in this problem. Whats my error here. 

标签 (1)
0 项奖励
回复
1 回复

807 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Would you please specify what was the problem during I2C write? no ACK? Please kindly clarify.

Thanks for your patience!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复