How to use NPN512 to communicate with Android Phone in p2p mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use NPN512 to communicate with Android Phone in p2p mode?

1,951 次查看
aviogg
Contributor I

I have no problems using RFID cards what so ever. I can read them and write on them. However, I have to use an Android Phone as a tag. For that I have been suggested 2 things. Either using a tag emulator to use phone as a basic tag, which is very hard, or use the p2p mode. 

My problem is that have found a library called nfcpy which makes everything very easy in terms of p2p communication but it does not support PN512(it support 532 and 522). 

Is there any library or kind of support to use p2p mode on this device?

(Sorry for grammar mistakes)

标记 (3)
2 回复数

1,743 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Nazım,

    PN512 and PN532 both support p2p mode , but PN522 doesn't support p2p. Our nxp official library for NFC supports p2p!

Hope the message can help you!

have a nice day!

Best regards,

Weidong

1,743 次查看
aviogg
Contributor I

Can you give me the link for this official library? Only thing I could come up with was some libraries about blueboard(which I have no idea what it is) and some others like these two:

NFC Reader Library v4.040.05 R2 for PNEV512B including all software examples

AN11308: Quick Start Up Guide PNEV512B Board

Thanks for the previous answer.

Best regards.

0 项奖励
回复