How to unlock PN7462?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to unlock PN7462?

Jump to solution
3,060 Views
jayesh_joshi
Contributor IV

Hi,

I am using the PN7462AU controller for NFC data transfer. I have downloaded firmware at 0x20A000 instead of 0x203000. After that I am trying to flash code at 0x203000 it is generating an error every time. I have tried erasing flash also but no success. This happens on two separate boards so the issue is critical. 

Thanks, Jayesh.

Tags (3)
0 Kudos
Reply
1 Solution
3,048 Views
nxf58474
NXP Employee
NXP Employee

Hi Jayesh,

 

Hope you are doing well. Could you please try to update the flash via USB Mass Storage Device interface? Section 8.10 of this User Manual.

 

Hope this helps.

 

Best Regards,

Ricardo

View solution in original post

0 Kudos
Reply
2 Replies
3,016 Views
jayesh_joshi
Contributor IV

Thanks @nxf58474 Ricardo

0 Kudos
Reply
3,049 Views
nxf58474
NXP Employee
NXP Employee

Hi Jayesh,

 

Hope you are doing well. Could you please try to update the flash via USB Mass Storage Device interface? Section 8.10 of this User Manual.

 

Hope this helps.

 

Best Regards,

Ricardo

0 Kudos
Reply