Hello @Fanfei
Hope you are doing well.
When you mention that the IC seems not to work, could you please describe the issue you are seeing?
Is there any chance you could provide a capture with an oscilloscope of the XTAL to try to check if it is working properly? Example of measurement of these signals is described in Crystal Oscillator Design Guide, Annex 2.
What is the procedure you are following to try to modify this EEPROM configuration? By any chance, are you using the recommended tool NFC Cockpit?
Perhaps you can try using the Load EEPROM feature of NFC Cockpit. This feature loads a previous saved file, and stores is into the user area of EEPROM; you could "Dump" a known-good EEPROM configuration from a working device.
Also, even though they are many, EEPROM has limited write cycles. Is it possible that you have a exceeded them?
Regards,
Eduardo.