How to reconfigure so that an NTAG213 chip cannot be read when password protected

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to reconfigure so that an NTAG213 chip cannot be read when password protected

1,227 次查看
tomtyrrell
Contributor I

Hi,

I wonder if someone could help on how to reconfigure pages within the NTAG213 chip so that the chip cannot be read when password protected? 

Is this even possible with this type of chip?

Any feedback will be highly appreciated.

Best Regards

Tom. 

标记 (1)
0 项奖励
回复
1 回复

1,007 次查看
elizabeth1
Contributor I

For setting also read protection you should set page 2A (PWD_AUTH) first byte to 1, so you will enable the read and write protection.

Anyway, after doing it, I have experienced a problem: my application set read/write protection by a password but I can't remove the password protection after that. If I just apply write protection I can remove it without any problem.

Hope it helps

Eli.

0 项奖励
回复