How to port the CLRC663 to IMX6 Android KitKat 4.4.2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to port the CLRC663 to IMX6 Android KitKat 4.4.2?

2,378 次查看
TracyZhang
Contributor I

HI all,

      We are using NXP's CLRC663 chip, the platform is Imx6q, and the system is kernel 3.0.35, Android 4.4.2.
I call the NFC library provided by NXP and compile the executable program, and I can read and write A and B cards.
I wanted to transplant it to Android 4.4, and no data was found. Only a set of pn54x transplants provided by NXP is found, as shown in the attachment.

I don't know how to transplant the following path.

How pn54x is transplanted into RC663.

Please help us, especially thanks!

├── external
│   └── libnfc-nci
│   ├── Android.mk
│   ├── CleanSpec.mk
│   ├── halimpl
│   │   ├── Android.mk
│   │   └── pn54x

0 项奖励
回复
2 回复数

1,957 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Tracy,

     Our NFC reader PN7150 & PN7120 are designed for those platform with OS, such as android , windows10 IOT, linux. And NFC lib-nci supports them.

    We didn't released CLRC663 solutions for android, So if you want to use NFC reader on your platform, PN7150 is strongly recommended for you.


Have a great day,
TIC  weidong sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,957 次查看
liyu1
Contributor III

Wigros Sun:

              CLRC663,这颗芯片用AN11690.pdf 这个文档里所说的,android4.4 里面的库能正常跑吗?

0 项奖励
回复