How to let CLRC663 board run without debug mode in MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to let CLRC663 board run without debug mode in MCUXpresso IDE

1,171件の閲覧回数
albertsung
Contributor I

Hi All,

I have the CLRC663 development kit (OM26630FDK) and it can work with the example codes in MCUXpresso IDE.

But if I disconnect the LPC-Link or if I only do the flash programming without debug mode in MCUXpresso IDE,

then the CLRC663 looks not working.

It seems it only can run with debug mode. Is there any method to run without debug mode ?

Best Regards,

Albert

 

タグ(3)
0 件の賞賛
返信
1 返信

962件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

What do you mean by not working? Do you have an error or something? which example you are using?  Could you please provide more details ? 

Regards

0 件の賞賛
返信