How to kill a NTag I2c Plus (or stop it)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to kill a NTag I2c Plus (or stop it)

863 Views
kaibuechler
Contributor II

Hello,

I'm using a NT3H2111 (QFN package) and commuincate with it over the i2c interface and a busy bee efm8b2 microcontroller. The NT3H2111 is supplied with 3.3v, has 3kOhm pull ups on sda and scl and 0.1uF capaictor next to its vcc pin. 

At first I did only read 7 Bytes of the config register (address 0x3A) just for testing the busy bee smbus driver. That test reading was running for at least a week or two, while I was working on other stuff. Today I started to develop the communction between the uC and the ntag, so the manual stated  that a i2c read and write config registers always transfers 16bytes. So I changed that from my 7byte to 16 and added a write accees to the config register ( stetting some values in the NC_REG at the config address, remaining bytes are kept to their default values). And this kills my ntag. I killed now the fourth chip, after I read more than the 7bytes and/or start writing the config reg. The chip dies after 4 or 5 times doing that. Looking on the SDA and SCL line then, they both are pulled to gnd when the uC tries to start the communiction. I can still access the ntag with my Smartphone (ndef data), but erase or wirting the config regsiters does not work either after the i2c communictation starts failing.

I measured everything around the ntag on my pcb, there is defenetly no shortcut, and 3kOhm pull ups should be fine also. And the test reading was running for at least a week, like I already stated. 

Has anyone faced a issue like that? I'm totally confused.

Labels (1)
Tags (2)
0 Kudos
1 Reply

551 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Could you please answer to the following questions so that we can help you in a more accurate way?

- What are the values you are trying to write to NC_REG?

- Do you do a power cycle (reset), those configuration registers gets mirrored into session regs. and these new settings are valid?

- You are mentioning that you set writing access conditions for I2C side. What precisely did you set (which byte to what value)?

- Are you by accident overwriting Byte0 on Page0 where I2C address of the NTAG is?

Regards,

Ivan.

0 Kudos