How to achieve the anti-counterfeiting function for IOS based on the NFC tag

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to achieve the anti-counterfeiting function for IOS based on the NFC tag

ソリューションへジャンプ
877件の閲覧回数
long19890829
Contributor II
As we know, the ios can only read the ndef message, and the ndef message is in the public area and is unencrypted, therefore, how could we identify the NFC tag is unique and is not a copy one, (except using the UID). Even, can we put a private key into the tag and the ios can get it, do you have a solution for this problem, and give us some advises.
One more question, for ICODE tag(Type 5, 15693), we would like to confirm which tag(specific model) support the UID and counter mirror features(mapping the UID and counter value into the ndef area);
looking forward your reply, and thank you very much!
Long
タグ(1)
0 件の賞賛
1 解決策
730件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear long zhu,

as you know IOS only supports reading to tags, and only to NDEF formatted tags, maybe you can store the UID as an NDEF text value and then read it, Until Apple supports more on NFC there not much that we can do here. please contact apple for more details on the NFC in IOS,  the following devices have UID please check the datasheets for more information on them.

ICODE DNA
SL2S6002FUD
ICODE SLIX 2
SL2S2602
ICODE SLIX
SL2S2002 / SL2S2102
ICODE SLIX-L
SL2S5002 / SL2S5102
ICODE SLIX-S
SL2S5302 / SL2S5402

BR

Jonathan

元の投稿で解決策を見る

0 件の賞賛
1 返信
731件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear long zhu,

as you know IOS only supports reading to tags, and only to NDEF formatted tags, maybe you can store the UID as an NDEF text value and then read it, Until Apple supports more on NFC there not much that we can do here. please contact apple for more details on the NFC in IOS,  the following devices have UID please check the datasheets for more information on them.

ICODE DNA
SL2S6002FUD
ICODE SLIX 2
SL2S2602
ICODE SLIX
SL2S2002 / SL2S2102
ICODE SLIX-L
SL2S5002 / SL2S5102
ICODE SLIX-S
SL2S5302 / SL2S5402

BR

Jonathan

0 件の賞賛