How do you put the MFRC630 in I2C fast mode+?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do you put the MFRC630 in I2C fast mode+?

1,046件の閲覧回数
robhelvestine
Contributor II

How do you put the MFRC630 in I2C fast mode+? It says it is supported, but doesn't describe how to enter this mode, instead of regular I2C speed. 

Thanks,

Rob

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

967件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Rob,

The device supports this mode in hardware, so no additional setup needed to enter this mode. Please refer to Fast Mode Plus - I2C Bus  for more details.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信