Hello,
A random Id can be enabled in this case. -Random ID can be set when PN7150 is configured in HCE
- in type A, LA_NFCID1 (NCI parameter Tag 0x33) must be set as zero length (while otherwise it is set as 4, 7 or 10 bytes length)
CORE_SET_CONFIG = "20 02 03 01 33 00"
- in type B, LB_NFCID0 (NCI parameter Tag 0x39) must be set as zero length (while otherwise it is set 4 bytes length)
CORE_SET_CONFIG = "20 02 03 01 39 00"
Hope this helps!
BR,
Ivan.