How can I protect a NTAG (NT3H2111) against ESD strike from NFC antenna

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I protect a NTAG (NT3H2111) against ESD strike from NFC antenna

Jump to solution
797 Views
aodzip
Contributor I

the question is the title.

I found PESD18VF1BSF , but the typical circut seems like a NFC "host".

Can PESD18VF1BSF protect a NFC "slave" device? If not , any suggestions? thanks

0 Kudos
1 Solution
607 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

ESD stress is applied on all pads of the IC. It meets the CDM and HBM specification of IC. All pins have the ESD protection built, so no special need for external diode.

Regards,

Ivan.

View solution in original post

2 Replies
606 Views
remoknuesel
Contributor I

Hello,

the pins are protected "only" up to 2kV HBM. What if one want to protect against IEC 61000-4-2 Level 3 (150pF, 330Ω, 8kV)?

We made tests with 5V ESD Diodes with a clamping Voltage of 20V without success.

Any advice?

Regards,

Remo

0 Kudos
608 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

ESD stress is applied on all pads of the IC. It meets the CDM and HBM specification of IC. All pins have the ESD protection built, so no special need for external diode.

Regards,

Ivan.