How can I obtain the FW source code for the LPC1769 on PNEV5180B board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I obtain the FW source code for the LPC1769 on PNEV5180B board?

1,942 次查看
ste
Contributor I

I need the source code of the FW loaded in the LPC1760 MCU on the PNEV5180B evaluation board. There are examples in the NFC RD library, but I need the code for the FW which communicates with the Cockpit test tool.

0 项奖励
回复
3 回复数

1,788 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Stefko Urumov,

You can find these binaries in “\NxpNfcCockpit_v4.8.0.0\firmware\Secondary_PN5180” folder.

VCOM firmware  binaries Cockpit.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,788 次查看
ste
Contributor I

Hi Robin!

Thank you for your reply !

I appreciate it, however, my request was specifically for the source code of the FW for the LPC1769 which allows the board to communicate to NXP NFC Cockpit tool.

Hopefully, this can be provided and it will help me to progress with the development of our products based on PN5180 and other NXP devices.

Stefko

0 项奖励
回复

1,788 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Stefko,

I am sorry to tell you that the source coude are not open to customers.

Best Regards,

Robin

0 项奖励
回复