Guideline to select DESFire Application ID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Guideline to select DESFire Application ID

259 Views
Ahlers
Contributor I

Hello,

I would like to create an application on a DESFire media. For that I have to select an application ID (AID). According my understanding I'm not restricted in the value of that ID. It just has to be in the range 1 to 0xFFFFFF. But it's also not possible to have two applications with the same ID on one media.

As I want to allow also other operators to put their apps on the same media I have to somehow make somewhat (many somes) secure that both use different AIDs. Of course we have "the first wins".

So is there any guideline which value could be used? Or are some ranges somehow reserved for something?

BR
Erwin Ahlers

0 Kudos
Reply
2 Replies

249 Views
Ahlers
Contributor I

I found AN10787 "MIFARE Application Directory (MAD)". This contains a proposal for AID selection. It includes also the information that I should register new classic application IDs. 

But this claccis application ID is a 2 Byte value where the higher value is already fixed as function cluster. So I have only one byte left as application code. That's not much.

So is MAD really used in practice? I haven't seen it until now, but have just a very narrow use of DESFire media until now.

BR
Erwin Ahlers

0 Kudos
Reply

231 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @Ahlers

Hope you are doing well.

MIFARE Application Directory (MAD) is a proposal; this may not be a mandatory process but it could be a good practice to register the AID so they are unique.

Regards,
Eduardo.

0 Kudos
Reply