Gerber file usage - AN11276

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Gerber file usage - AN11276

跳至解决方案
2,381 次查看
EthanMathew25
Contributor III

Hi, 
Can I use the Gerber files provided along with NXP NTAG I2C NFC IC as it is without making any modifications to them ?
Can I use them on different substrates ? how much performance degrade will be there ? How to overcome those ? 

标记 (3)
0 项奖励
回复
1 解答
2,254 次查看
Tomas_Parizek
NXP Employee
NXP Employee

Hello,

Ok, it should be fine. 

Anyhow, once you produce the antennas, it is recommended to measure them with the help of the VNA and potentially tune the tag by a parallel capacitor as shown below. 

Tomas_Parizek_0-1707201529860.png

BR

Tomas 

 

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,316 次查看
Tomas_Parizek
NXP Employee
NXP Employee

Hello EthanMathew25

Do you mean the following files located in AN11276?

Tomas_Parizek_0-1706606231071.png

BR 

Tomas

0 项奖励
回复
2,304 次查看
EthanMathew25
Contributor III
yess! those files...
can I use them on any substrate or do I have to make any changes?
0 项奖励
回复
2,271 次查看
Tomas_Parizek
NXP Employee
NXP Employee

Hello EthanMathew25, 

What substrate are you planning to use? 

Yes, as the antenna turns are only on one layer, the different substrates should not have any major impact. 

We typically use a standard FR4 or Flex. 

BR

Tomas 

 

2,264 次查看
EthanMathew25
Contributor III
Polyimide substrate
0 项奖励
回复
2,255 次查看
Tomas_Parizek
NXP Employee
NXP Employee

Hello,

Ok, it should be fine. 

Anyhow, once you produce the antennas, it is recommended to measure them with the help of the VNA and potentially tune the tag by a parallel capacitor as shown below. 

Tomas_Parizek_0-1707201529860.png

BR

Tomas 

 

0 项奖励
回复
2,354 次查看
EthanMathew25
Contributor III

@Tomas_Parizek Help me out...

0 项奖励
回复