Flash Magic issues with NSH3100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash Magic issues with NSH3100

3,143件の閲覧回数
shadyelmakhzang
Contributor I

Hello everybody,

 

I am using the Flash magic V10.96.4956 to download a Hex file on an NHS3100 throuh the SWD over Link2 interface. I have two boards that faces a different kind of issues:

 

1- The first board states that "Failed to read the device signature (Operation Failed. (reading signature)). Accessing a device using the wrong protocol could render the device unsuable. Do you want to continue?"

The debugging file for this board is flashmagic-20180622-075751.fmd.

 

2- The other board states that "Operation Failed. Failed to autobaud - step1."

The debugging file for this board is flashmagic-20180622-080218.fmd.

 

Can anybody help me?

 

Thanks,

Shady R. Elmakhzangy

0 件の賞賛
返信
4 返答(返信)

2,811件の閲覧回数
vrushali_b
Contributor I

Hi,

I am facing same issue with flashing NHS3152 using flash magic. "Failed to read the device signature (Operation Failed. (reading signature)). Accessing a device using the wrong protocol could render the device unsuable. Do you want to continue?"

Did you resolved this issue?

0 件の賞賛
返信

2,811件の閲覧回数
driesmoors
NXP Employee
NXP Employee

Hi vrushali.b@snsystems.in‌, 

I suspect the target device is still set to NHS3100, as in the screenshot posted by Kan‌ above. When flashing an NHS3152 IC, you can change the target device by clicking on the Select... button on the left.

Kind regards,
Dries.

0 件の賞賛
返信

2,811件の閲覧回数
driesmoors
NXP Employee
NXP Employee

Hi,

FlashMagic is a third party tool, and support for this can be obtained via http://www.flashmagictool.com/support.html or by emailing support@esacademy.com. I think the debugging files you attached make sense to them only.

The SDK currently promotes v10.90, as that was the version the images were tested with at the time of release of SDK 11.1 BETA. You can download past installers of Flash Magic via http://www.flashmagictool.com/download.html

I'm now using the latest version of Flash Magic - v11.16 - and this is working fine for my needs.

The two errors you listed seem to stem from the same problem. I suspect the board is not being powered (did you fit a jumper over JP2?) or being in / going to Power-off or Deep Power Down mode.

  • Have a look at <SDK>docs/AN_NHS31xx_Flashing.pdf > 2.2 Flash Magic, especially the note at page 12.
  • When developing, also have a look at <SDK>/docs/firmware.html > SW Debug Considerations

In short, it boils down to making sure the IC is awake when the IC is contacted through the SWD lines.

Kind regards,
Dries.

0 件の賞賛
返信

2,811件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Shady,

I am sorry, but I could not reproduce your issue here, and I am using 10.9 , and I have JP2 on LPC-Link 2 installed.

pastedImage_1.png

pastedImage_2.png


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信