Felica card support in PN7150

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Felica card support in PN7150

821 Views
sivasu4098
Contributor III

Hi all,

  I have successfully ported PN7150 in my custom hardware (msm8909) which is running under Android Nougat. How to enable Felica card support in PN7150. Please provide the documents or libraries needed for porting Felica card support.

Regards,

Sivasubramaniyan P

Tags (3)
0 Kudos
1 Reply

659 Views
nxf58474
NXP Employee
NXP Employee

Hi Sivasubramaniyan P,

 

Hope you are doing well.  Sorry for the inconvenience this might cause you, but we do not provide migrations of the NXP NFC Reader library.

Nonetheless,  we do have some guides you help you in the process, the first thing I would recommend you to check would be the NFC Reader Library webinar to understand the structure of the library.

 

Also I might suggest to take a look in the following community thread and use the information of this  repository as a reference for your migration. It might help you with your project.

 

Let me know if you have further questions.

0 Kudos