Does NFC reader library support more than one IC on bus?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does NFC reader library support more than one IC on bus?

757 次查看
inspirionlake
Contributor I

Hi! I'm working on device with two PN5180 ICs on SPI bus.

I want to clear: it is possible to use NFC reader library with more than one ICs on bus, when both ICs should working concurrently? (It means that cards can appear in the both fields in the same time)

In the library I see:

1) Global variables (phNfcLib_Initialization.c):

phNfcLib_DataParams_t gphNfcLib_Params;
phNfcLib_InternalState_t gphNfcLib_State;

2) Restriction in library's documentation for function: 

phNfcLib_Status_t phNfcLib_SetContext(phNfcLib_AppContext_t * pAppContext)

that it should be called before calling phNfcLib_Init()

All this above (1) & (2) made me thinking that internal architecture of NFC reader library doesn't support working with several ICs in one firmware design, please correct me if I'm wrong.

 

Best regards

标签 (1)
0 项奖励
回复
0 回复数