Difficulties about download to nhs3100. Ep(01) Ee(36)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difficulties about download to nhs3100. Ep(01) Ee(36)

770 Views
yys3210
Contributor II

Dear NXP developers :

I am  working on   app_demo_dp_tlogger.

HW:  nhs3152 demo board;   lpc-link2 

SW:  LPCXpresso(V8.2.0)   ,(release    redlib(nohost)    Og )

When i  trying to  download to the target  with LPCXpresso,I will get error messages as shown below:

Sometimes  02 failed on connect:Ep(01) target marked as not debugable 

 

  sometimes   02 failed on connect:Ee(36) could not connect to core

 pastedImage_1.png

BTW  after init() function in the main() , I  wrote about 11 bytes to EEPROM  at offset  64 .

I had  tried  to  push reset button , and it does not work.

I am anxious to get your reply

0 Kudos
2 Replies

639 Views
yys3210
Contributor II

There are some more questions:

Q1,If  I want to store some  datas (less than 20) to eeprom permanently ,where can i write to?  

Q2, where does the tags stored ?

Q3.If  the chips are damaged ,how can i  solve it ?

THANKS 

0 Kudos

639 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

It would be helpful to check the get started guide available in the following link: Get Started with the NHS3152THADADK | NXP 

For detailed memory read/write information, please refer to section 8.22 until 8.24.2 of the datasheet.

For any related situation with your product, please contact your distributor.

BR,

Ivan.

0 Kudos