Confirmation of PN7362 protocol issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Confirmation of PN7362 protocol issues

796 Views
Karyliu
Contributor II

Hi NXP,

There is a diagram in PN7150datasheet that reads and writes Sony FeliCa according to ISO/IEC18092 standard. This illustration is not available on PN7362.

But in the selection table, it is written that PN7362 supports ISO18092 and FeliCa. It is uncertain whether PN73262 follows ISO18092 when reading and writing FeliCa cards on the USB CCID interface?

Thank you.

0 Kudos
Reply
1 Reply

735 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

Unfortunately,we do not provide complete support for Felica cards. Our reader library is capable of detecting Felica cards and activate them, all additional tags' operations shall be implemented by customers, in case you require more information about Felica's commands, please contact Sony support.

 

 

Regards

Daniel

0 Kudos
Reply