Chip mifare nxp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Chip mifare nxp

1,322件の閲覧回数
ricardosandoval
Contributor I

Hi,

I 'm looking into that as much information other than characters fits in a mifare nxp chip , it is possible guaradar a fingerprint or a photograph ?, in 1k or 4k or 8k ? currently they have a tool to record information in their chips ( mifare 1k , 2k, 8k ) ?

best regards

0 件の賞賛
返信
1 返信

1,151件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Ricardo Sandoval:

In the fingerprint case, I am not familiar with the algorithms used to digitally store fingerprints, but I do not think that it fits in a Mifare card.

About the photograph, in a 8K Mifare card you could include a small jpeg picture as part of a vCard record (business card) in a Base64 format. Another option is to write a separate record with a dedicated image MIME type just for the picture. However for bigger files it is not usual to include them in the card, but instead write a URI to an online site containing the complete file.

There are several tools to store records in NFC cards. For example the TagWriter application developed by NXP is free of charge, please watch the next video about it:

NFC TagWriter App by NXP|NXP

I hope this helps.

Regards!

Jorge Gonzalez

0 件の賞賛
返信