Change key for the NTAG 424 DNA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change key for the NTAG 424 DNA

2,399 Views
shaghayeghnz
Contributor II

Hi, 

I'm currently experiencing some issues with changing the key for the NTAG 424 DNA. According to the document at https://www.nxp.com/docs/en/application-note/AN12196.pdf, specifically in section 6.16.2, if I authenticate with keyNo 01, I should be able to change keyNo 01. However, when I run the command, I receive the response 91AEh, which, according to the document at https://www.nxp.com/docs/en/data-sheet/NT4H2421Gx.pdf, means "At the application level, missing active authentication with the AppMasterKey while targeting any AppKey."

BR, Shaghayegh.

0 Kudos
Reply
4 Replies

2,343 Views
GlennN
Contributor I

Hi, This reply does not really answer the question, shaghayeghnz wants to change the key data not change which key is to be used. I am also trying to do this and cannot get it to work with TagXplorer.

My problem is similar but not identical (https://community.nxp.com/t5/NFC/NTAG424-ChangeKey-not-working-in-TagXplorer/m-p/1748722/emcs_t/S2h8...

 

I am sure we would both be grateful for any help

 

0 Kudos
Reply

2,335 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @GlennN 

Please take a closer look. The key has also been changed. In my test example, the values of key4 and key5 are different.

BR

kelly

0 Kudos
Reply

2,327 Views
GlennN
Contributor I

@KaiLiYes, sorry, I had missed the change of value in Key 5

0 Kudos
Reply

2,376 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @shaghayeghnz 

Yes, you're right. Once you authenticate with keyNo 01, and then keyNo 01 can be changed by ChangeKey command. The below test log for your reference.

KellyLi_0-1698053056053.png

BR

kelly

0 Kudos
Reply