Hi,
I'm currently experiencing some issues with changing the key for the NTAG 424 DNA. According to the document at https://www.nxp.com/docs/en/application-note/AN12196.pdf, specifically in section 6.16.2, if I authenticate with keyNo 01, I should be able to change keyNo 01. However, when I run the command, I receive the response 91AEh, which, according to the document at https://www.nxp.com/docs/en/data-sheet/NT4H2421Gx.pdf, means "At the application level, missing active authentication with the AppMasterKey while targeting any AppKey."
BR, Shaghayegh.
Hi, This reply does not really answer the question, shaghayeghnz wants to change the key data not change which key is to be used. I am also trying to do this and cannot get it to work with TagXplorer.
My problem is similar but not identical (https://community.nxp.com/t5/NFC/NTAG424-ChangeKey-not-working-in-TagXplorer/m-p/1748722/emcs_t/S2h8...
I am sure we would both be grateful for any help