Capacitor rating for PN5190

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Capacitor rating for PN5190

621 Views
jr_hernandez
Contributor II

Hi,

I need to confirm the voltage rating for capacitors in matching network for PN5190 EVB (PNEV5190B).

The BOM in the design files is not fully detailed with commercial part numbers so I can not find compatible parts.

I think they are rated to 250V because a collegue could open the source altium file, but I need confirmation asap because we would like to use 0603/0402 instead of 0805.

One question:

Why do matching capacitors in CLEV6630B_V2.0 are rated to 50V and 250V for PNEV5190B if both Front Ends are specified to have 2W?

Please, provide fulll detailed BOM for PNEV5190B base board at your earliest convininence.

Regards, Ramon.

 

 

 

 

0 Kudos
Reply
0 Replies