According to AN11742.pdf Fig. 3, the measured AGC value should rise with a card moving closer to the reader.
I have a piece of code, that constantly reads 0x26, without writing to it.
To my understanding, this should perform a quick AGC reading.
What strikes me is that the value gets lower with a card moving closer, not higher.
The values hover around AGC Gear 0, AGC Value 300.
Card absent: ~310
Card fully in contact: ~290
This seems like a fairly small variability...
Here are the questions that arose:
1. Why is the AGC value getting lower, not higher with the card moving in?
2. Why is the AGC value variability so low? Is 10 +- enough to trigger LPCD?
3. Should the mechanism theoretically switch to a gear with a higher variability?
For completeness, here is my EEPROM readout, with the DPC regs. It seems to be turned on, but my AGC is not getting high enough to switch gears, I think:
73 DPC_CONTROL DPC enabled, step size 1, start gear 7
20 4e DPC_TIME 20000 / 1ms
00 DPC_XI
40 25 AGC_CONTROL duration 320, duration enable, step size 0, step size enabled
72 01 73 01 72 01 6e 01 66 01 63 01 5d 01 4e 01 90 01 ad 00 a7 00 9e 00 96 00 87 00 4a 00 DPC_THRSH_HIGH
370, 371, 370, 366, 358, 355, 349, 334, 400, 173, 167, 158, 150, 135, 74
00 00 DPC_THRSH_LOW
00 DPC_DEBUG
05 DPC_AGC_SHIFT_VALUE
09 DPC_AGC_GEAR_LUT_SIZE
f9 f1 f3 f5 f7 f0 f2 f4 f6 96 66 46 36 26 16 DPC_AGC_GEAR_LUT
20 4e DPC_GUARD_FAST_ MODE
a8 61 DPC_GUARD_SOF_ DETECTED
90 01 DPC_GUARD_FIELD_ON
5d 91
Thanks for any hints!
Hello @dakhnod
Please see the comments as the below:
1. Why is the AGC value getting lower, not higher with the card moving in?
Which is related the threshold.
2. Why is the AGC value variability so low? Is 10 +- enough to trigger LPCD?
AGC value variability will not trigger LPCD, LPCD needs to be abled via command.
3. Should the mechanism theoretically switch to a gear with a higher variability?
A card is entered into the antenna field, which increases the load, and therefore the output power. As soon as the measured AGC value exceeds the AGC high threshold value of the corresponding gear (DPC_THRSH_HIGH), the PN5180 (resp. PN7462) automatically switches to the next gear with lower output power. This automatically reduces the measured AGC value, until the card is moved closer to the antenna.
Hello,
thanks for taking the time.
I understand that the chip should be switching gears by itself anf exit LPCD, if configured so.
Yet, my question still stands: Why is the AGC value getting lower upon inserting a card, without the gear switching?
Thanks!