Can PN7642 chip run without an external 3.3v?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can PN7642 chip run without an external 3.3v?

650件の閲覧回数
AgungWib
Contributor I

Hi,

 

I want to ask, whether PN7642 can be run without an external 3.3v LDO?

I read on the datasheet PN7642 has internal LDO for 3.3v.

So I'm asking to reduce the BOM cost can we run PN7642 without any external 3.3v LDO, we only provided with 5V supply voltage to VBAT, VDDPA, VUP_TX, etc.. ?

 

Thanks!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

631件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @AgungWib 

The PN7642 has an LDO output pin PVDD_OUT which can be enabled via the configuration registers. It's recommended to refer to the Table 454 of UM11566. U11566 is a security file, so you need to sign an NDA with NXP and then have accessing rights.

0 件の賞賛
返信