Can I buy the NFC module on OM5577?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I buy the NFC module on OM5577?

1,435 Views
sangdolee
Contributor I

Hi,

I made a prototype product using OM5577. But, OM5577 board is too big for my product.

But, NFC module's size on OM5577 is good for us.

Do you know where I can buy this NFC module, not OM5577 board?

BR

Paul

0 Kudos
Reply
3 Replies

1,350 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to the following link in the BUY/PARAMETRICS section:

PN7120|NXP 

Regards,

Ivan.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,350 Views
sangdolee
Contributor I

Thanks, Ivan.

0 Kudos
Reply

1,350 Views
IvanRuiz
NXP Employee
NXP Employee

Hi Sangdo Lee,

You are welcome.

Have a great day!

Regards,

Ivan.

0 Kudos
Reply