Hello,
I have a question about the HTRC110. Can it write/read T5577 RFID tags? I'm currently doing a project where I have to design a reader/writer for these tags.
Hope you can help me.
Thanks in advance.
Best regards,
Arend
Hi all,
I'm also designing a reader for NLIS cattle tags (Passive RFID transponder). As it is mentioned above HTRC110 won't be a help. Is there any other reader IC that I can use for my purpose?
Transponder :
* Compatible with ISO 11785 & 11784
* In HDX
* 30mm diameter
* Passive RFID
Hi Arend Wierks,
The HITAG Reader ICs are optimized and designed to work with HITAG transponder ICs (HITAG|NXP ) compliant with ISO 11784/85 or ISO 14223 standards. Since T5577 is a third party card type then I cannot say if the reader will work with such card. Sorry for the inconvenience.
Regards!
Jorge Gonzalez
Dear Jorge,
I can't find the antenna design guide for HTRC110 on NXP Website. Can you share it to me?
Application note AN98080 includes the information about antenna design for HTRC110
http://www.nxp.com/documents/application_note/AN98080.pdf
Regards!
Jorge Gonzalez