Dear Support,
We have the experience with using NFC Reader Library v06.10.00, going with NXP/ST32L 32-bit ARM MCU and runs very well.
Now we have a new project need to use 8051 8-bit MCU with the reader IC CLRC663. Now we are trying to porting NFC Reader Library to 8051 8-bit MCU platform and meet lots errors and issues to go through. Before, we have used RC522 with 8-bit MCU is OK, but it seems the latest reader IC CLRC663 is hard to work with 8-bit MCU.
The code size of NFC Reader Library is more than 50KB, it consumes most of 8-bit MCU flash memory, which is up to 64KB memory size.
Do you have customers use 8-bit MCU to work with CLRC663? If so, did they use NFC Reader Library? Or the use below suggestion?
Using the RC663 without library (nxp.com)
It looks like the without-library-solution only supports small portion of functions that NFC Reader Library can support.
If you have customers can implement NFC Reader Library by using NXP 8-bit MCU, can you tell us what are the MCU? So that we can refer to design in our reader?
Thanks~
Best Regards,
David Huang