Calculating CMAC for DESFire EV1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Calculating CMAC for DESFire EV1

3,039 Views
david_cleal
Contributor I

I'm working through the examples in AN0945. I'm stuck on table 41, trying to understand how to calculate AES CMACs.

In step one, it says 

...Calculate CMAC on “3D01000000100000010203040 50607080910111213141516” (cmd + file no + offset + length + data) as done in native mode.

I used my CMAC implementation to correctly calculate the CMAC on this as 7CC4A0C770A11F62762F397482F75E92, using the session key, which gives me some confidence that my CMAC implementation is correct. 

However, in step 5, it says

...Calculate CMAC on “00” (success code as in native)... and it says that the result should be 99FF486D1BCE3F24.

I assume this means I should get a 16 byte CMAC and these are the first eight? In any case, if I calculate the CMAC on "00" using the session key of 00112233F9B7C14CCCDDEEFF1E92CBD4, I get something completely different (I actually get 5C0821A202813197E29134F30CF3728D).

So, my question is, does the calculation actually work on just "00"? Is there some other difference between steps 1 and 5? For example, I don't believe that I should use the IV in the CMAC calculation, but perhaps I should?

Thanks in advance

- Dave

Tags (2)
0 Kudos
6 Replies

1,041 Views
giraffe508
Contributor IV

Response: Dear AtekPayments,

 

Here's a simple pseudocode for generating CMAC, CRC32, and CRC16:

 

1. CMAC Generation:

```

function generate_cmac(key, message)

    // Initialize the CMAC context with the given key

    cmac_context = init_cmac_context(key)

 

    // Update the CMAC context with the message

    update_cmac_context(cmac_context, message)

 

    // Finalize the CMAC context and get the result

    cmac_result = finalize_cmac_context(cmac_context)

 

    return cmac_result

end function

```

 

2. CRC32 Calculation:

```

function crc32(data)

    crc = 0xFFFFFFFF

 

    for each byte in data

        crc = update_crc32(crc, byte)

    end for

 

    return crc ^ 0xFFFFFFFF

end function

 

function update_crc32(crc, byte)

    crc = crc ^ byte

 

    for i = 0 to 7

        if crc & 1

            crc = (crc >> 1) ^ 0xEDB88320

        else

            crc = crc >> 1

        end if

    end for

 

    return crc

end function

```

 

3. CRC16 Calculation:

```

function crc16(data)

    crc = 0xFFFF

 

    for each byte in data

        crc = update_crc16(crc, byte)

    end for

 

    return crc

end function

 

function update_crc16(crc, byte)

    crc = crc ^ byte

 

    for i = 0 to 7

        if crc & 1

            crc = (crc >> 1) ^ 0xA001

        else

            crc = crc >> 1

        end if

    end for

 

    return crc

end function

```

 

Please note that these are simple pseudocode examples and may need to be adapted to your specific programming language and use case

0 Kudos

2,444 Views
david_cleal
Contributor I

Quiet in here, isn't it?

In case anyone comes this way,  then I found the answer, which is that yes, you do use the IV in the CMAC calculation. But not in the bit where you use the cipher to calculate sub keys, just in the final encryption pass. This makes it difficult to do this using bouncy castle, and I ended up rolling my own CMAC implementation. After that, everything just worked.

0 Kudos

2,443 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear David Cleal,

I deeply apologize for the delay,  yes you will have to use the updated IV for future calculations not the zeros IV, so the calculations should be 

Data = 00
IV = 7CC4A0C770A11F62762F397482F75E92

Session Key = 00112233F9B7C14CCCDDEEFF1E92CBD4

and the result should be 99 FF 48 6D 1B CE 3F 24 60 69 D8 4D 03 38 55 A6.

Hope this is clear and please let me know if you have more questions.

BR

Jonathan

0 Kudos

1,102 Views
AtekPayments
Contributor I

Can you provide me with sample sudo code for cmac generation also CRC32 & CRC16

0 Kudos

2,444 Views
david_cleal
Contributor I

Dear jonathaniglesias

thanks for the message - as I said earlier, I did manage to get it working, once I realised we were using a modified IV. Incidentally, varying the IV seems like pointless complexity: it makes it harder to use standard implementations like bouncycastle, and it doesn't add security. But I guess it's way too late to complain ;-)

- Dave

0 Kudos

2,444 Views
david_cleal
Contributor I

Update... I can't even make the example in table 24, step 4, work. Is there a reference implementation of this calculation somewhere that I can use? Preferably in Java?

0 Kudos