CLRC663 with NTAG212

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663 with NTAG212

1,257 Views
chadgraham
Contributor V

Hello,

I have a CLRC663+ dev kit and I'm trying to communicate with a NTAG212.  (Specifically, it is an antenna/chip component that uses the NTAG212 as the TAG chip.)  I am able to communicate with a MIFARE card using the instructions from the dev kit user manual, but this isn't working for the NTAG212.  Is there a different sequence of events that I can use to confirm that the reader can communicate with the tag?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,174 Views
nxf58474
NXP Employee
NXP Employee

Hi chadgraham@cogmedix.com,

 

Hope you are doing well. Which MIFARE are you able to communicate with? You can see the Communication Principle of the NTAG212 in section 8.4 of the Data Sheet.

 

The CLRC663 plus is able to communicate with the NTAG212, as the reader supports the ISO/IEC 14443A , and the tag is designed to fully comply ISO/IEC14443 Type A specifications.

 

Best Regards,

Ricardo

0 Kudos
Reply