CLRC663 plus and RS232 Tx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663 plus and RS232 Tx

703 Views
M_Chene
Contributor II

Hello everyone,

I am trying to use a CLRC663 plus communiacting in RS232 with a MK20 µC. When I look the RX pin (IF0) with an oscilloscope I can observe the good communication frame (Sa, Address[0x7F],RD, So), but TX (IF2) stays at HIGH state...

IFSEL0 and 1 are set to ground and IF3 is connected to VDD according to the table in the evalboard's schematic. My communication speed is set to 115.2 Kb/s and I use a MAX3221 as level shifter.

Do you have any idea to this matter ?

Thanks in advance

 

Mathieu

Tags (3)
0 Kudos
2 Replies

693 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

That seems there is no the question of the CLRC663 depending on the datasheet as the link.

URL:https://www.nxp.com/docs/en/data-sheet/CLRC663.pdf.

That should be  related to the serial communication characteristics of kinetis . You may confirm it with  the kineti s engineers on kinetis community.

Hope it help you.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 Kudos

686 Views
M_Chene
Contributor II

Thank you for your answer,

I am sure that the  serial part of the MK20 is not the problem because it can do rs232 communication with others components I use. I made a diagram of how I connected my CLRC. Does this seem OK for you or did I misunderstand something in the datasheet on the RS232 connection (IF3 is connected to VDD and IFSEL pins to GND)?

RS232CLRC.png

Another thing that I want to verify is the frame I send. In the picture I wanted to read Command register (0x00). In yellow there is the signal in the RS232 part and in blue it is the signal between the MAX3221 and the CLRC663 plus

DS0029.BMP

Does this frame seems good to you or must I send something before (it is the first time I use this component, so I don't think it is in Standby mode)?

 

Thank you in advance for your help.

Best regards

 

Mathieu

0 Kudos