CLRC663 layout on a multilayer stack

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CLRC663 layout on a multilayer stack

355 次查看
dramos
Contributor I

Hi to all,

I am designing a 6 layer pcb with the #CLRC663. After reading the Application Note AN11019 (rev 1.5), in the chapter 3.2 Layout recommendation there is a mention about the GND plane under the CLRC663 evaluation board. The GND plane is in middle layer of the board

On the SW4301 - CLEV6630B v2.0 PCB,there is not copper under the matching circuitry. 

As I mentioned before, I have a multilayer board and I would like to know if I can place a GND plane under the matching components (Matching components Layer1-GND Layer2). Can I have traces under the matching components in the other layers? For example layer 3 or Layer 6? 

Or should I remove all the copper under the matching components in all layers of my stack?

Thanks for your comments.

david

 

标签 (1)
0 项奖励
回复
2 回复数

348 次查看
Tomas_Parizek
NXP Employee
NXP Employee

Hello @dramos 

We typically keep a first GND layer under matching as shown below. This is mainly due to EMI reasons. 

matching_GND.jpg

BR

Tomas 

0 项奖励
回复

338 次查看
dramos
Contributor I

Hi Tomas,

Firstly thanks for your response. 

If below the matching circuit I place a GND plane for EMI control , is it necessary to remove the copper area in the rest of the layers? 

In my case I am using a 6 layers stack, if the matching is in the first layer and the GND in the second I think that I shouldn't remove the copper on the other four layers. The demo board is not made in that way and I cannot understand why.

Any idea about the best procedure?

Thanks to all 

david

0 项奖励
回复