HI,
I'm currently tring to make our CLRC663 based board working with ILT-M tags.
For that, I get some part of code in the NxpNfcRdLib_07.05.00 and other part in code provided in SW335613.
The RFLibrary is not suitable as it cannot help to perform inventory of many tags.
SW335613's Inventory_18000p3m3 is more suitable for this purpose. However please note that the code for Q adaptation is not working as the line fQ = round(fQ) (line 172) is not correct. Q will never change if C is lower then 0.51. This line should be removed.
Whatever, with all settings from NxpNfcRdLib_07.05.00 and algorithm based upon SW335613 I have very poor RF performances with the sample tags I get from you.
Same board is working well up to 6cm range with ISO15693 tag but only 0.5 with ILT tags. This is very disappointing.
How much power does an ILT tag require ?
Does an ILT tag required such power that it is not suitable to be used with standard desktop RF reader with small antenna ?
Regards