CLRC663 Plus in place of the CLRC663 not Plus and extendign the operating distance ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663 Plus in place of the CLRC663 not Plus and extendign the operating distance ?

492 Views
cant
Contributor II

How to extend the operating distance using the "CLRC663 Plus (CLRC66303xxx) " on an already developed board with "CLRC663 not Plus (CLRC66302xxx)" ?

Thanks a lot

0 Kudos
1 Reply

443 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

According to specs, the Plus version of CLRC663 has an improved output current on the transmission, which is called ITVDD, where ITVDDmax = 350 mA under loading conditions. In theory, if you switched the Frontend from the "Not-Plus" to the Plus version, you will not notice any improvement since the matching has been done for the same target impedance, in this case for the previous CLRC663.

It would be helpful to please refer to the Antenna design App Note for reference about changing the target impedance for better performance: https://www.nxp.com/docs/en/application-note/AN11019.pdf 

Hope this helps!

BR,

Ivan.

0 Kudos