Hello,
I'm implementing an Android HCE based use case using a CLRC663 in LPCD configuration to wake up an embedded system by means of a smartphone. In my implementation I have an ARM M4 micro connected to the CLRC663. I'm implementing the ISODep RFID stack using NXP NFCRdLib.
Is there any way using NFCRdLib to detect when it's the right time to put in sleep the micro and to minimize the time from wakeup to end card activation?I did some tries, launching phacDiscLoop_Sw_Run(), then phhalHw_Rc663_Cmd_Lpcd() and then putting the micro in sleep. What I got is that it takes about 800ms to wake up doing a first discovery and 900 ms to finally activate the card (smartphone in card emulation). What I see on the smartphone is a delay of about 2 s from the moment I put it near the reader and the moment the smartphone is aware of NFC communication. Is there a way to speed up the process? Am I doing something wrong? Is there any sample code I can study to implement my use case?
Thanx
Hi,
We provide an example of NfcrdlibTst12_Rc663Lpcd for CLRC663 , did you test with this demo? what type of card did the phone simulate in your test? Please kindly clarify.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------