Hello,
quick question about the MFRC522. We are using a custom build antenna. Would connecting the antenna is only to one of the two TX pins work? Or do I need to connect an antenna to both TX1 and TX2?
Hello.
>>Would connecting the antenna is only to one of the two TX pins work?
Yes, If the customer build antenna supports it.
I send the related design to you via email. Please check it .
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------