Hi, I was wondering whether or not there would ever come support for the PN5180 NFC reader in Zephyr. I am very interested in combining NXP’s IMXRT1064, PN5180 and Zephyr. Are there any prospects of adding the NFC reader library in Zephyr or adding support for Zephyr in the NFC reader library? Thanks!
Hello,
Unfortunately. Zephyr can't support PN5180. For the more information please refer to the information as the link.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------