I am writing regarding the doc AN11755 Antenna design guide of PN7150 https://www.nxp.com/docs/en/application-note/AN11755.pdf
Some figures are incomplete, e.g. Fig 44 and Fig 51. Is there an updated version?
Regards
Ahmed
Hello,
Unfortunately, There is not the updated version for it so far. the version 1.7 is the latest version. Thanks for your understanding.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------